Channels View

The Channels page shows an overview of the configuration values for all module channels. The values for each channel indicate how that particular channel is configured on that channel’s page. You can change certain configuration parameters in this view, not all of them.
TIP: To view or change the complete set of the channel configuration, use Chxx view.
Channels View Example

Chxx Views

The Chxx views are displayed based on the channel modes configured in the Channel Assignments tab under Device Definition dialog.
Available Chxx views are:
  • Chxx - Digital Output
  • Chxx - Digital Input
  • Chxx - Counter
  • Chxx - Digital Input, Timestamp
  • Chxx - IO-Link
  • Chxx - Digital Input, Fallback
  • Chxx - Digital Input, Timestamp, Fallback
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal