Chxx - Digital Input, Timestamp View
This view is available when the channel is configured as “Digital Input, Timestamp”. You
can perform certain tasks only when the project is online.
Use this view to complete the following tasks:
- Select the Input Filter Time.
- Capture timestamps for Input transitions.
- Enable or disable Timestamp Latching.
- Enable or disable Chatter Detection.
- Configure the Chatter Detection options.
- Access the channel diagnostics.
Chxx - Digital Input, Timestamp View Example

Provide Feedback