Module Configuration
Before you start configuring your I/O module, you must create a Studio 5000 Logix
Designer application project for the Logix 5000 controller that owns the PointMax I/O
modules. See Add a New Module to a Studio 5000 Logix Designer Application Project for more
information.The project includes module configuration data for the PointMax I/O
modules.
The Studio 5000 Logix Designer application transfers the project to the owner-controller
during the program download. Data is then transferred to the PointMax I/O modules when
the connection is established. The PointMax I/O modules can operate immediately after
receiving and applying the configuration data.
Provide Feedback