Chxx - Digital Input, Fallback View

This view is available when the channel is configured as “Digital Input, Fallback”. You can perform certain tasks only when the project is online.
Use this view to complete the following tasks:
  • Enable or disable the channel.
  • Select the Input Filter Time.
  • Access the channel diagnostics.
  • Access the port-level IO-Link event log.
  • Disable and Delete the master copy of the Data Storage on the IO-Link port.
Chxx - Digital Input, Fallback View Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal