Chxx - Digital Output View

This view is available when the channel is configured as “Digital Output, Short Circuit”, or “Digital Output, Short Circuit, No Load”. You can perform certain tasks only when the project is online.
Use this view to complete the following tasks:
  • Select the Program Mode and Communication Fault Mode Output states.
  • Enable or disable No Load Diagnostics (only available when the channel is configured as “Digital Output, Short Circuit, No Load”).
  • Access the channel diagnostics.
Chxx - Digital Output View Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal