Chxx - IO-Link View
This view is available when the channel is configured as “IO-Link”. You can perform
certain tasks only when the project is online.
Use this view to complete the following tasks:
- Enable or disable the channel.Use this checkbox to disable the channel temporarily to:
- Stop IO-Link communication for safety considerations. For example, when you change the channel mode from “IO-Link” to “Digital Output”.
- Disable Data Storage for the IO-Link port to prevent unexpected Data Storage Backup/Restore operation. Data Storage is re-enabled on the IO-Link port when the connection to the device is established again.
- Access the channel diagnostics.
- Access the port-level IO-Link event log.
- Disable and Delete the master copy of the Data Storage on the IO-Link port.
Chxx - IO-Link View Example

Provide Feedback