Chxx - Digital Input View
This view is available when the channel is configured as “Digital Input”. You can perform
certain tasks only when the project is online.
Use this view to complete the following tasks:
- Select the Input Filter Time.
- Access the channel diagnostics.
Chxx - Digital Input View Example

Provide Feedback