Chxx - Counter View

This view is available when the channel is configured as “Digital Input, Counter”. You can perform certain tasks only when the project is online.
Use this view to complete the following tasks:
  • Select the Input Filter Time.
  • Enable or disable Counter Rollover at Preset.
  • Access the channel diagnostics.
Chxx - Counter View Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal