Base controls
    Use base controls objects to implement user interface elements that enable interaction with the application.
| Object | Description | 
|---|---|
| Displays text that describes an item. | |
| Inserts and displays text at runtime. | |
| Increases or decreases a numerical value using buttons or keys. | |
| Displays an editable description of an item. | |
| Displays a Boolean value in the form of an on LED or an off LED. | |
| Generates events to perform methods. | |
| Sets and displays a Boolean value. | |
| Sets and displays a Boolean value using select and clear. | |
| Selects a mutually exclusive option in a group. | |
| Sets or displays an integer value within a range of possible values. | |
| Sets or displays an integer value within a range of possible values. | |
| Displays date and time data in a specific input format. | |
| Displays the duration data. | 
base control
    
Provide Feedback