Switch

Sets and displays a Boolean value.

Use case

Enable or disable functions or features within a
FactoryTalk Optix Application
. For example, toggle a graph that visualizes data.

Example

Disabled switch with optional text
Animated graphic showing a sliding switch control toggling from ON to OFF
Enabled switch with optional text
Animated graphic showing a sliding switch control toggling from ON to OFF
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal