Circular gauge

Sets or displays an integer value within a range of possible values.

Use case

Set and display an analog variable value within a minimum and maximum value.
TIP: Use the
Warning zone
property to display specific ranges of values in different colors.

Example

Circular gauge with two warning zones defined
animated graphic showing the circular gauge measurement moving between 0 and 90
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal