Delayed button

Generates events to perform methods. Includes a MouseLongPress event.

Events

Use these button events to trigger methods:
Event
Generated at runtime when
MouseLongPress event
An object is clicked or touched for the time specified in the
Delay
property.
MouseClick event
An object is clicked or touched and then released.
MouseDown event
An object is clicked or touched.
MouseUp event
The click or touch of the object is released.

Example

Default delayed button
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal