Toggle button
Generates events to perform methods. Includes a Modified value event.
Events
Use these button events to trigger methods:
Event | Generated at runtime when |
|---|---|
Modified value |
|
MouseClick event | An object is clicked or touched and then released. |
MouseDown event | An object is clicked or touched. |
MouseUp event | The click or touch of the object is released. |
Example
Default toggle button

Provide Feedback