Switch Channel Mode from IO-Link or Fallback to Digital Output
WARNING:
If the channel mode is IO-Link or Fallback,
the IO-Link master module periodically generates a wake-up pulse. If an output device is
connected to the channel, it may trigger an unexpected action from the device.
- Go online with your project.
- Go to IO-Link master Module Properties → Connection, clear the Inhibit module checkbox and select Apply.If Apply changes warning appears, select Yes.
- Go to IO-Link master Module Properties → Channels → Chxx - IO-Link or Fallback, select the Disable Channel checkbox and select Apply.IMPORTANT: The project must be online and the connection to the IO-Link master module must be uninhibited when you select Apply to enable or disable the channel. Otherwise the enable or disable channel request is not sent to the master module.If Apply changes to module configuration warning appears, select Yes without inhibit.
- Go offline with your project.
- In the IO-Link master Module Properties → Overview → Device Definition → Channel Assignments, change the channel mode from the Selected Mode dropdown list to a Digital Output.
- Select OK. If Apply changes warning dialog appears, select Yes.
- Connect the output device to the IO-Link master module.
- Go online with your project.
Provide Feedback