Recommended Maintenance Schedule Task Descriptions
Task | Description |
---|---|
Inspect | Inspect the component for signs of excessive accumulation of dust, dirt, or external damage. For example, inspect the filters/fan inlet screens for debris that can block the airflow path. |
Clean | Clean the components that can be reused, specifically the door-mounted air filters and fan inlet screens. |
Maintain | This type of maintenance task can include an inductance test of line reactors/DC links, or a full test of an isolation transformer, and so on. |
Replace | This component has reached its mean operational life. Replace the component to decrease the chance of failure. It is likely that components can exceed the designed life in the drive, but component life is dependent on many factors such as usage and heat. Use the predictive maintenance parameters to determine a replacement schedule for components in shaded table rows. |
Review | Self-review or a discussion with Rockwell Automation personnel is recommended to help determine whether any of the enhancements/changes made to the drive firmware or hardware could benefit the application. |
Provide Feedback