Remove and Install the Stirring Fan Assembly - Frame 6
Replace a stirring fan assembly with kit catalog number SK-RM-MFAN1-F6. Follow these steps to remove and install the stirring fan assembly.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Remove the cover from the chassis. See Remove and Install the Frame 6 Cover.
- Disconnect the fan power wire harness connectors (A) from the connectors on the chassis.
- Loosen the M4 captive screw that secures each of the fan assemblies to the chassis.
- Slide the fan assembly away from the chassis until the mounting tabs (B) align with the holes in the fan mounting plate, and remove the fan assembly.
- Install the stirring fan assembly in the reverse order of removal.
Provide Feedback