Remove and Install the Heatsink Fan Assembly - Frame 6
Replace a heatsink fan assembly with kit catalog number SK-RM-HSFAN1-F6. Follow these steps to remove and install the heatsink fan assembly.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Remove the cover from the chassis. See Remove and Install the Frame 6 Cover.
- If installed, remove the conduit box. SeePowerFlex®755T Frames 5 and 6 Conduit Box and Ground Plate Kits, Installation Instructions, publication 750-IN112.
- TIP: The heatsink fan power wire harness is connected inside the chassis. You cannot remove the fan assembly until you disconnect the fan power wire harness.
- Loosen the four M4 captive screws that secure the fan assembly to the chassis and carefully pull the fan assembly away from the chassis, partially.
- Disconnect the fan power wire harness connector (A) from the connector inside the chassis and remove the fan assembly.
- Install the heatsink fan assembly in the reverse order of removal.
Provide Feedback