Remove and Install the DR and PE-A (EMC and MOV) Jumper - Frame 6
Replace the DR and PE-A (EMC and MOV) jumper with kit catalog number SK-RM-JMPR1-F6. Follow these steps to remove the DR and PE-A (EMC and MOV) jumper.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Remove the cover from the chassis. See Remove and Install the Frame 6 Cover.
- Loosen the three captive, slotted-Torx head screws that secure the jumper to the power interface circuit board.
- Lift the jumper away from the power interface board until the keyholes in the jumper align with the pins on the sidewall and remove the jumper.
- TIP: The PE-A jumper is shown in the default (IN) position.
- Install the DR and PE-A (EMC and MOV) jumper in the reverse order of removal.
- Verify that the jumper is installed in the correct position as required for your grounding scheme and application. See the PowerFlex 750-Series Products with TotalFORCE Control, Installation Instructions, publication 750-IN100, for jumper configuration.
Provide Feedback