Connection View

Use Connection to define controller-to-device behavior:
  • Set the RPI rate. For more information, see Requested Packet Interval.
  • Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
  • View the reason of Connection Fault.
    TIP: If there is a connection fault, Connection Fault area displays the error code with description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
  • Inhibit the module. For more information, see Module Inhibiting.
  • Configure fault response for connection failure while the controller is in Run Mode.
  • Enable or disable the Automatic Diagnostics.
    ATTENTION: If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FatoryTalk Alarms and Events.
Connection View Example

Recommended Minimum RPI Values for Notch Filters

In the following table, each Notch Filter setting has recommended minimum module RPI value that allow the required time to collect samples from each channel. The recommended minimum RPI for the module is the maximum one of all recommended values per channel.
Notch Filter and Recommended Minimum Module RPI Values
Notch Filter (Hz)
Recommended Minimum Module RPI Value
10
106
20
53.1
50
22
60 (default)
18.3
100
9
200
5.9
500
2.2
1000
1.1
2500
0.5
5000
0.3
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal