Requested Packet Interval
Requested Packet Interval (RPI) is a configurable parameter that defines a specific rate
at which data is exchanged between the controller and the module.
You set the RPI value during initial module configuration and can adjust it as necessary
after module operation has begun.
IMPORTANT:
If you change the RPI while the project is
online, the connection to the module is closed and reopened in one of the following
ways:
- You inhibit the connection to the module, change the RPI value, and uninhibit the connection.
- You change the RPI value. In this case, the connection is closed and reopened immediately after you apply the change to the module configuration.
Provide Feedback