Modbus Slave View
    Use Modbus Slave view to configure settings for Modbus communication as a Master
            slave.
Modbus Slave View Example

| Parameter | Definition | Available Choices | 
|---|---|---|
| Modbus Format | Determines whether the Modbus transmission format is Modbus RTU
                                    or Modbus ASCII. | 
 | 
| Node Address | Specifies the node address of the slave. | 1…247 (default = 1) | 
| Diagnostics | When the controller status is online, open the Diagnostics dialog
                                    to view diagnostic counters for performance and error management
                                    with the Modbus Slave.  | – | 
Select Diagnostics to see the diagnostic information of the Modbus Slave channel.
Modbus Slave Channel Diagnostics Dialog Example

Provide Feedback