Controller Organizer

The
Controller Organizer
window is a graphical representation of the contents of your project that you can resize, undock, dock, and move. It contains a hierarchy of the folders, files, and links that contain information about the programs and data in the current project. For detailed information about the structure of the
Controller Organizer
, see:
In front of each folder that has content, there is an icon that indicates whether the folder or item is expanded or collapsed. Select the icon to expand the item.
TIP:
When you close the open project or the
Logix Designer
application, the last known expansion states for all high-level folders within the
Controller Organizer
are saved and stored. The
Controller Organizer’
s high-level folders are:
  • Controller <name>
  • Tasks
  • Motion Groups
  • Alarm Manager
  • Assets (Trends, Add-On Instructions, Data types)
I/O Configuration
Right-clicking an item opens a context-sensitive menu for that item. Commands on the menu are shortcuts to the item's
Properties
dialog box and menu bar commands. Double-clicking a file in the
Controller Organizer
opens the
Properties
dialog box.
TIP:
The
I/O Configuration
folder displays a Module Fault icon if a module below it is faulted.
The
Quick View
pane under the
Controller Organizer
tree provides summary information about the selected item in the
Controller Organizer
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal