Move items in the Controller Organizer

Move items from their original location to a new location under a new parent item in the following ways:
  • Cut and paste to move it with the mouse or the keyboard.
  • Drag-and-drop the item with the mouse.
  • Select multiple items to move at the same time.
    TIP: if FactoryTalk Security is enabled, FactoryTalk Security permissions are required to create and delete items in the
    Controller Organizer
    and the
    Logical Organizer
    .
For additional navigation information, see:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal