Danger: Unscheduling programs online affect logic execution

You are attempting to unschedule a program or programs while the system is online by dragging them to the
Unscheduled Programs / Phases
folder in the
Controller Organizer
. Unscheduling programs while online changes the execution of programs and may have unintended consequences.
Select
OK
to unschedule the program(s), or click
Cancel
to leave the program(s) scheduled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal