FactoryTalk®
Remote Access™ Manager Tools
FactoryTalk®
Remote Access™
ManagerFactoryTalk®
Remote Access™
Tools consist of three applets:
- Interactive Access: It allows to establish and manage a VPN, serial or USB device connection. Furthermore, it provides an overview of the connected devices.NOTE: See Interactive Access to learn how to navigate this tool and manage device connections and settings.
- Device setup: It allows to discover and register a new device that you wish to control remotely to a domain, and manage any router settings and connections.NOTE: See Device Setup to learn how to get started with the router discovery and settings management.
- Connection settings: It allows to set the connection port and proxy server type. These settings are used for establishing a VPN connection between theand the devices registered to the domain.FactoryTalk® Remote Access™ManagerNOTE: See Connection Settings to learn how set a device connection.
NOTE:
See FactoryTalk Remote Access Manager Tools installation and FactoryTalk Remote Access Manager Tools for further information on this subject.
After installation
Once you have installed the Tools on your device, you can access them as described in their related section FactoryTalk Remote Access Manager Tools, or directly by clicking their icons, if you are familiar with their use:
- Device discovery: This icon triggers the device discovery forOptixEdge™,OptixPanel™featuring a firmware version 4.0.4 or newer,Alternatively, you can refer to Device Setup to discover a device throughStratix® 4300featuring a firmware version newer than 4.0.2 and Embedded Edge Compute Module featuring a firmware version 4.0.4 or newer..FactoryTalk® Remote Access™Manager
- Local Connection: This icon allows to establish the Local Connection connection mode. See Local connection if you want to establish this connection mode through.FactoryTalk® Remote Access™Manager
Provide Feedback