FactoryTalk®
Remote Access™ Manager Tools installation
FactoryTalk®
Remote Access™
ManagerFactoryTalk®
Remote Access™
ManagerAccess the and select to download all the Tools.
FactoryTalk®
Remote Access™
Manager
NOTE:
See Tools
for further information on this subject.
NOTE:
See FactoryTalk Remote Access Manager Tools to learn more information about the
Tools.
Tools can be installed on the following operating systems:
- Windows 10 x64
- Windows Server 2016, 2019 and 2022
Once installed, the Tools are ready for use.
NOTE:
Whenever you access a Tool that requires update, a message window will appear, asking you whether you want to proceed with downloading its updated version.
NOTE:
To set up your language, see Language setup
After installation
Once you have installed the Tools on your device, you can access them as described in their related section FactoryTalk Remote Access Manager Tools, or directly by clicking their icons, if you are familiar with their use:
- Device discovery: This icon triggers the device discovery forOptixEdge™,OptixPanel™featuring a firmware version 4.0.4 or newer,Alternatively, you can refer to Device Setup to discover a device throughStratix® 4300featuring a firmware version newer than 4.0.2 and Embedded Edge Compute Module featuring a firmware version 4.0.4 or newer..FactoryTalk® Remote Access™Manager
- Local Connection: This icon allows to establish the Local Connection connection mode. See Local connection if you want to establish this connection mode through.FactoryTalk® Remote Access™Manager
Provide Feedback