System Architecture Examples

Runtime entitlements are based on the number of feature tokens that your application requires. The examples that are given in this section are typical applications; your own architecture can be different than what is shown.
Package sizes:
  • XS - extra small; up to five tokens
  • S - small; up to eight tokens
  • M - medium; up to 11 tokens
  • L - large; up to 15 tokens
  • XL - extra large; up to 21 tokens
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal