Station Runtime (XL)

This XL example shows you a system architecture using an HMI and two web clients.
XL System architecture
A diagram of sample XL system.
This example architecture has the following components:
  • Single HMI station with typical HMI functionality and 20 web clients
  • Communicates with multiple
    Rockwell Automation®
    controllers and multiple third-party controllers
  • Acts as a client to multiple OPC UA servers
  • Acts as an OPC UA server to one client
  • Logs data to an internal database
  • Exchanges data with external databases via ODBC
  • Requires event logging, alarming, recipes, and basic PDF reporting
The following picture shows example runtime sizing for a package that includes these application components.
HMI with Extensibility
An example runtime sizing for a package in an XL system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal