Station Runtime (L)
This L example shows you a system architecture using an HMI and two web clients.
L System architecture
This example architecture has the following components:
- Single HMI station with typical HMI functionality and ten web clients
- Communicates with multipleRockwell Automation®controllers and multiple third-party controllers
- Acts as a client to other OPC UA servers
- Logs data to an internal database
- Requires event logging, alarming, recipes, and basic PDF reporting
The following picture shows example runtime sizing for a package that includes these application components.
HMI with three web clients and OPC UA

Provide Feedback