Terminology
This table defines terms that are used in this publication.
Term | Definition |
|---|---|
Activate a FactoryTalk®
Hub™ Entitlement | The process of either assigning an entitlement to a runtime target
device or a myRockwellAutomation User. The process is the same to
upsize an existing entitlement. Activation is typically performed by The myRockwellAutomation User
who is a member of the FactoryTalk®
Hub™
organization to which the entitlement is allocated. |
Advisor | A cloud-based platform for product selection, configuration, bill of
materials management, and more. Available through FactoryTalk®
Hub™ . |
Allocate a FactoryTalk®
Hub™ Entitlement | After purchase of a FactoryTalk® Optix™ or FactoryTalk®
Remote Access™ entitlement, you must allocate the
entitlement to the appropriate FactoryTalk Hub organization before
it can be used. The myRockwellAutomation User who placed the order on the Rockwell
Automation Software Commerce Portal typically allocates the
entitlement. |
Application Code Libraries/Trusted Content | Preconfigured content that is developed, managed, and made available
from Rockwell Automation at no additional cost to help expedite
project creation and project maintenance. |
Container | A containerized software deployment. A container is a way to package
an application and its requirements into one unit, making the
application portable and easier to manage. See FactoryTalk Optix Studio Applications as Container Solution. |
Devices with Optix embedded | Specific Runtime Target Devices that come from Rockwell Automation® preloaded with the software and entitlements for FactoryTalk® Optix™ Runtime Tools and FactoryTalk® Remote Access™ Runtime. Access to the operating system in these devices is
restricted (closed system).See Table 1. |
Entitlement | The license that is required to run FactoryTalk®
Hub™ software, such as FactoryTalk® Optix™ and FactoryTalk®
Remote Access™ . |
FactoryTalk Design Studio® | A cloud-based design platform that enables teams to work on projects
involving multiple controllers. Available through FactoryTalk®
Hub™ . |
FactoryTalk®
Hub™ | A cloud-based platform, which serves as a central access point for
Software-as-a-Service (SaaS) offerings. FactoryTalk®
Hub™ is accessible via www.FactoryTalkHub.com and
requires a MyRockwellAutomation account to sign in.Some FactoryTalk®
Hub™ products require the purchase of a license to operate. |
FactoryTalk®
Hub™ Organization | An organization acts as a grouping for myRockwellAutomation Users,
licenses, and access rights within FactoryTalk®
Hub™ , which enables collaboration and resource sharing. It is free to create or join an organization and required to use FactoryTalk®
Hub™ . |
FactoryTalk® Optix™ | A cloud-enabled Human Machine Interface and IIoT platform. Available
through FactoryTalk®
Hub™ . |
FactoryTalk® Optix™ Application | The project that is developed in FactoryTalk® Optix Studio™
and compiled to run. |
FactoryTalk® Optix™ Entitlement | Available in several package sizes consisting of a quantity of
feature tokens. The entitlement can be upsized to a larger package size
at any time. Also available as perpetual entitlement with maintenance
or a subscription. A perpetual entitlement is included with some
runtime target devices with an optional one-step upsize of the
perpetual entitlement available. See Table 1. |
FactoryTalk® Optix™ Runtime Tools | FactoryTalk® Optix™ runtime software that is used to run a FactoryTalk® Optix™ Application. |
FactoryTalk® Optix Studio™ | FactoryTalk® Optix™ design-time software |
FactoryTalk® Optix Studio™ Entitlements | Available in two options: Standard (free) or Pro (paid
subscription). |
FactoryTalk®
Remote Access™ | A cloud-based solution that enables secure remote connectivity to
industrial automation equipment. Available through FactoryTalk®
Hub™ . |
FactoryTalk®
Remote Access™ Manager | A web-based interface for managing remote connections to industrial
automation systems with a FactoryTalk®
Remote Access™ Runtime. |
FactoryTalk®
Remote Access™ Manager Entitlement | Available as a subscription based on the number of concurrent users.
The number of concurrent users is how many users can connect to
remote devices simultaneously, not the total number of users that
can use the software. |
FactoryTalk®
Remote Access™ Runtime | Software that allows you to establish secure, remote connections to
industrial equipment from the FactoryTalk®
Remote Access™ Manager. |
FactoryTalk®
Remote Access™ Runtime Entitlement | Available as a perpetual entitlement or a subscription. In either
Basic or Pro levels. A perpetual entitlement is included with some
hardware. Upsizing from Basic to Pro is available. See Table 1. |
Feature Tokens | The number of feature tokens determines the size of a FactoryTalk® Optix™ Runtime Entitlement. See Table 1. |
myRockwellAutomation | A centralized user access platform from Rockwell Automation® that provides a personalized
experience by bringing together a wide range of digital tools and
resources, including product information, software subscriptions,
support documentation, Knowledgebase articles, and more. |
myRockwellAutomation User | The email address that is registered with myRockwellAutomation. |
Offline | The runtime target computer is not on a network that can be routed to
FactoryTalk®
Hub™ . |
Online | The runtime target computer is on a network that can be routed to FactoryTalk®
Hub™ .Examples of online scenarios:
|
Purchase |
|
Rockwell Automation Software Commerce Portal | Also known as the Subscription Portal, compliments Rockwell
Automation’s network of authorized distributors by serving as a
centralized ecommerce platform for software purchases, subscription
management, and more. Access to the Rockwell Automation Software
Commerce Portal requires a MyRockwellAutomation account
to sign in.
|
Runtime Target Computer | Specific Runtime Target Device that is either an ASEM™ 6300 industrial computer or any PC or
virtual machine that runs Windows® or Linux
operating system. Access to the operating system in these devices is
not restricted (open system). |
Runtime Target Device | The compute device that you use to run the FactoryTalk® Optix™ Application. Types of Runtime Target Devices include:
See Table 1. |
Software-as-a-Service (SaaS) | A software distribution model that allows access to software through
a web browser or app instead of installing and managing software on
a PC or device. |
Virtual Machine | Virtual version of a physical computer, which allows multiple
operating systems and applications to run on one physical
computer. |
Provide Feedback