Runtime Sizing Calculator
The Runtime Sizing Calculator lets you enter the details of your project
and recommends the feature token package that you need (see Table 1).
To determine
the runtime package that you need for your application, use the Runtime Sizing calculator within the
FactoryTalk® Optix™
page on FactoryTalk®
Hub™
.- SelectFactoryTalk® Optix™from the list of available applications.

- Select Runtime Sizing from the top navigation bar.

- Follow the wizard to select the features your application needs.
After you complete the wizard, you are provided with the package size needed and the
associated software catalog number for purchase via the Commerce
Portal. Some target devices from Rockwell Automation come with the
FactoryTalk® Optix™
Runtime entitlement included (see Table 1).Provide Feedback