Runtime Entitlements
A Runtime entitlement lets you access and run the
FactoryTalk® Optix™
Application in a Microsoft®
Windows®
or Linux environment. You can select the
Runtime entitlement that aligns to the specific requirements of your application.
Runtime entitlements are sold in packages that include Feature Tokens. Different Runtime features are assigned a feature token value, so that any set of features
can be used in an application. The application features and total feature tokens used define
the Runtime entitlement size required. For more information on sizing your application, see
Runtime Sizing Calculator and Example Runtime Entitlements.Provide Feedback