FactoryTalk Optix Runtime download and installation
Before installing the Runtime, use the Runtime Sizing calculator to determine the size
FactoryTalk® Optix™
Runtime Tools package that you need.- IMPORTANT:Runtime Tools are already embedded in OptixPanels™ and EECM (Embedded Edge Compute Modules).You have to download, install and activate Runtime Tools for Windows and Linux devices.
- Depending on your device OS, Activate a FactoryTalk Optix Runtime entitlement on Windows devices or Activate a FactoryTalk Optix Runtime entitlement on Ubuntu 22 devices.
TIP:
To rehost a
FactoryTalk® Optix™
Runtime, see Rehost a Runtime entitlement on Windows devices or Rehost a Runtime entitlement on Ubuntu 22.04 devices, depending on your
device OS.You can launch the
FactoryTalk® Optix™
Runtime and use it without any entitlement for two hours. After this time, you need to purchase an entitlement and allocate it to your organization.
IMPORTANT:
Runtime is already embedded in OptixPanels™ and EEC (Embedded Edge Computes).
You have to download, install and activate Runtime Tools for Windows and Linux devices.
IMPORTANT:
If you uninstall Runtime Tools, the next time you log in your application will automatically restart. You cannot deploy an application after Runtime Tools are uninstalled because the uninstall removes the Update Service.
Provide Feedback