Start FactoryTalk Optix Studio Pro

Once an entitlement has been allocated, you can launch
FactoryTalk® Optix Studio
Pro from either your desktop or a web browser, having the Pro features enabled in either way.
TIP: You can use
FactoryTalk® Optix Studio
Pro if you have been assigned an entitlement or granted a 90-day trial period.
  • Launch
    FactoryTalk® Optix Studio
    Pro from your desktop
    :
    TIP: Despite the application icon on the desktop remains unchanged, the Pro features will show up upon valid user login and entitlement allocation.
    1. In the Windows
      Start
      menu, start typing
      FactoryTalk Optix Studio
      or double-click the
      FactoryTalk® Optix Studio
      icon on your desktop.
    2. Once the application opens, if you are not signed in, select
      Sign in
      from the top bar and sign in with your MyRockwellAutomation account credentials.
    3. If you made any changes to your entitlements while working with
      FactoryTalk® Optix Studio
      , restart the application.
  • Launch
    FactoryTalk® Optix Studio
    Pro from a web browser
    :
    1. Access the
      FactoryTalk® Optix
      landing page. See FactoryTalk Optix landing page.
    2. Authenticate as required.
    3. On the
      FactoryTalk® Optix
      landing page, select
      Open in Browser
      .
      TIP:
      If you do not have an entitlement for
      FactoryTalk® Optix Studio
      Pro, a dialog displaying
      Entitlement required
      opens.
      Complete
      Name
      ,
      Email
      , and
      Description
      and then select
      Submit
      .
      You will receive an email to grant you a trial entitlement when your request is approved. Approval can take up to 24 hours. You can download and install the desktop version of
      FactoryTalk® Optix
      until your
      FactoryTalk® Optix
      Pro entitlement is approved. When the entitlement is available, repeat the steps above.
    4. Select
      Continue
      to launch
      FactoryTalk® Optix Studio
      TIP:
      Selecting
      Cancel
      keeps the
      FactoryTalk® Optix
      landing page open.
      To automatically open
      FactoryTalk® Optix Studio
      Pro from your last session, select the avatar with your initials in the upper right corner of the landing page, and then in
      Settings
      , select
      Auto open last used workspace
      and select
      Save
      .
      TIP: Once you launch
      FactoryTalk® Optix Studio
      Pro from a browser once, it automatically launches the next time you open the
      FactoryTalk® Optix
      landing page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal