Activate a FactoryTalk Optix Runtime entitlement on Windows devices
Activate a Runtime Tools entitlement to launch the application on the Runtime device.
TIP:
A runtime device running Windows can have multiple licenses. Each runtime
device is associated with one of the available entitlements.
- Select the WindowsStartmenu and start typingEntitlement Manageror double-click theFactoryTalk® Optix Studio™icon on your desktop.
- InEntitlement Manager, underInstalled entitlements, select the entitlement type:
- Online: Activate an online entitlement.
- Offline: Activate an offline entitlement.
Provide Feedback