Manage target devices

Add, remove, duplicate, and select target target devices available in the network.
The default target target device, the
Emulator
, runs locally on the development computer. The
Emulator
is useful for testing
FactoryTalk Optix Applications
and does not require you to install the
FactoryTalk Optix Application Update Service
software.
TIP: The
Emulator
runtime stops automatically after two hours even if a valid license is present on the device. If you need to test your application for a longer period of time, export the application. See Export a FactoryTalk Optix Application.
TIP: Rebooting the
Emulator
is not supported so that you do not accidentally reboot a device on which
Windows®
is installed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal