Select a target device

Select an already configured target device to deploy
FactoryTalk Optix Applications
over the network to the target device.
  1. From the main toolbar, next to
    Run
    , select the target dropdown menu.
  2. (optional) In
    Target device settings
    , to display only the active remote target devices, toggle
    Active remote devices
    .
    TIP: Refresh remote target devices by selecting
    Refresh
    .
  3. Select a target device.
  4. Choose
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal