Remove a target device
Remove target devices that you no longer need.
- From the main toolbar, next to, select the target dropdown menu.Run
- (optional) InTarget device settings, to display only the active remote target devices, toggleActive remote devices.TIP: Refresh remote target devices by selectingRefresh.
- Select a target device.
- SelectRemove the selected target device.
- In theTarget device settings, selectRemove.
Provide Feedback