Configure the Adapter

After you install the EtherNet/IP adapter and set the IP address, you must add the adapter to a controller project. The project must be online to set the Speed and Duplex configurable parameters on the module.
IMPORTANT:
You must use the Studio 5000 Logix Designer application version 36 or later.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal