Configure the Ethernet Port Settings

If you did not already configure the Ethernet port speed and duplex settings with FactoryTalk Linx software, complete these tasks:
  1. Put the controller mode switch in the REM position.
  2. Change the Studio 5000 Logix Designer application project to Run Mode.
    When prompted to change the controller mode to Remote Run, select Yes.
  3. Right-click on your adapter, and select Properties.
  4. From the Device Information view, select Port Configuration.
    Desired Task
    Action
    Let the module automatically set the port speed and duplex settings.
    Leave the Auto-Negotiate checkboxes selected.
    Manually configure your port speed and duplex settings.
    Follow these steps:
    1. Clear the Auto-Negotiate checkbox.
    2. Under Speed category Selected column, select the port speed from the dropdown list.
    3. Under Duplex category Selected column, select Full from the dropdown list to set the port to full-duplex mode.
  5. From the Module Properties view, select Internet Protocol.
    If needed, you can set Internet Protocol properties such as:
    • Domain Name
    • Host Name
    • Gateway Address
    • Primary DNS Server Address
    • Secondary DNS Server Address
  6. On the Module Properties dialog, select OK.
    IMPORTANT:
    If you try to change the IP address on this page, the following alert appears:
  7. Save the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal