IntelliCENTER

The IntelliCENTER software provides a window into your Motor Control Center (MCC). The IntelliCENTER extension is customized for your IntelliCENTER MCC to provide extensive virtual representation of your entire IntelliCENTER MCC lineup. The extension also provides critical IntelliCENTER MCC information such as a Spare parts list, Drawings and User Manuals.
Features of IntelliCENTER include:
  • A graphical representation of your entire MCC lineup in the Elevation view.
  • Customized views of your IntelliCENTER MCC documentation, including manuals, CAD drawings, and a spare parts list.
  • Monitor the status of an MCC lineup in the IntelliCENTER Explorer Tree, Elevation view, or Dashboard by entering the network paths of the devices within the MCC to monitor and then starting or stopping status monitoring.
    Each device that supports Ethernet IP provides one of these statuses: , , , , or .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal