IntelliCENTER Dashboard

Access the IntelliCENTER Dashboard to:
  • Import a new lineup.
  • Export a lineup.
  • Edit a network path.
  • Start and stop a lineup's status monitoring.
  • Monitor the lineup's overall status.
Access the
IntelliCENTER Dashboard
from the explorer bar. Select Devices Icon
Devices
, then the
IntelliCENTER
tab. Select
IntelliCENTER Dashboard
on the bottom.
On the
IntelliCENTER Dashboard
:
  • View a list of lineups and associated serial numbers.
  • Import a new lineup.
    1. Select
      Import new lineup
      .
    2. Select
      Browse
      under
      Databases
      to import datasets. Or select
      Browse
      under
      Documentation
      to import MCCs with documentation associated with it.
    3. Select one or more of the lineups and select
      Upload
      to import the datafiles into FactoryTalk Design Studio.
  • Export a lineup.
    1. Select the box select mcc lineup associated with the lineup you want to export.
    2. Select the
      Export lineup
      option. The
      Export MCC Lineup
      dialog box opens.
    3. Select
      Download
      to download the zipped data set to the computer's
      Downloads
      folder.
  • Edit a network path.
    1. Select the box select mcc lineup associated with the lineup you want to edit the network path.
    2. Select the
      Edit Network Path
      option. The
      Edit Network Path
      dialog box opens.
    3. Add or edit the network paths. For more information, see Add a VPN driver.
  • Start and stop a lineup from status monitoring by toggling the slide to the right to start monitoring the lineup or to the left to stop monitoring the lineup.
  • Monitor the lineup's overall status by viewing the lineup's
    Status
    column. The
    Status
    column represents the most significant status in the lineup. If the lineup's status monitoring is not enabled, the status reads .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal