Import an MCC lineup

Import MCC lineups from datasets purchased with IntelliCENTER MCCs documentation associated with it (post-shipment) or without documentation associated with it (pre-shipment).
Prerequisites
  • Purchase and download the dataset folder.
  • Unzip the dataset folder to your local drive.
To import an MCC lineup
In FactoryTalk Design Studio:
  1. Open or create a project.
  2. Select
    File > Import > MCC lineup
    to open the
    Import MCC Lineup
    dialog box.
    1. To import an MCCs dataset, under
      Databases
      , select
      Browse
      to locate the dataset folder on your local drive.
    2. To import MCCs lineup documentation, under
      Documentation
      , select
      Browse
      to locate the folder on your local drive.
      TIP: You have the option to browse for both databases and documentation and add them to the lineup in one import step.
  3. Select one or more of the lineups and select
    Upload
    to import the datafiles into FactoryTalk Design Studio.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal