FIFO Unload (FFU)

The FFU instruction unloads the value from position 0 (first position) of the FIFO and stores that value in the Destination. The remaining data in the FIFO shifts down one position.
Use the FFU instruction with the FFL instruction to store and retrieve data in a first-in/first-out order.
When enabled, the FFU instruction unloads data from the first element of the FIFO and places that value in the Destination. The instruction unloads one value each time the instruction is enabled, until the FIFO is empty. If the FIFO is empty, the FFU returns 0 to the Destination.
Typically, the destination and the FIFO are the same data type. If the types differ, the instruction converts the unloaded value to the type of the destination tag.
A smaller integer converts to a larger integer by sign-extension.
Available Languages
Ladder Diagram
Ladder Diagram_FIFO Unload (FFU)_v1
Operands
There are data conversion rules for mixed data types within an instruction.
Ladder Diagram
Operand
Type
Format
Description
FIFO
SINT
INT
DINT
REAL
String type
structure
array tag
FIFO to modify
Specify the first element of the FIFO
Do Not use CONTROL.POS in the subscript
Destination
SINT
INT
DINT
REAL
String type
structure
tag
Value unloaded from the FIFO.
Control
CONTROL
tag
Control structure for the operation
typically use the same CONTROL as the associated FFL
Length
DINT
immediate
Maximum number of elements the FIFO can hold at one time
Position
DINT
immediate
Next location in the FIFO where the instruction loads data
initial value is typically 0
CONTROL Structure
Mnemonic
Data Type
Description
.EU
BOOL
The enable unload bit indicates the FFU instruction is enabled. The .EU bit is set to prevent a false unload when the prescan begins.
.DN
BOOL
The done bit is set to indicate that the FIFO is full (.POS = .LEN).
.EM
BOOL
The empty bit indicates the FIFO is empty. If .LEN is , or = to 0 or .POS < 0, the .EM bit and .DN bits are set.
.LEN
DINT
The length specifies the maximum number of elements in the FIFO.
.POS
DINT
The position identifies the end of the data that has been loaded into the FIFO.
Affects Math Status Flags
No
Major/Minor Faults
A major fault will occur if:
Fault Type
Fault Code
The specified Length is past the end of FIFO array
4
20
See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition / State
Action Taken
Prescan
See FFU Flow Chart (Prescan).
Rung-condition-in is false
See FFL Flow Chart (False).
Rung-condition-in is true
See FFU Flow Chart (True)
Postscan
N/A
FFU Flow Chart (Prescan)
FFU Flow Chart Prescan
FFL Flow Chart (False)
RSL5K_FFL Flow Chart False
FFU Flow Chart (True)
FFU Flow Chart True
Examples
Example 1
Ladder Diagram
FTStudio-FFU-LD-EX1-V1
RSL5K_FFU Example 1
Example 2
Destination array is STRING array or Structure array
Ladder Diagram
FTStudio-FFU-LD-EX2-V1
Example 3
Data type of FIFO source array mismatch data type of destination array
Ladder Diagram
FTStudio-FFU-LD-EX3-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal