FIFO Load (FFL)

The FFL instruction copies the Source value to the FIFO.
Use the FFL instruction with the FFU instruction to store and retrieve data in a first-in/first-out order. When used in pairs, the FFL and FFU instructions establish an asynchronous shift register.
Typically, the Source and the FIFO are the same data type.
When enabled, the FFL instruction loads the Source value into the position in the FIFO identified by the .POS value. The instruction loads one value each time the instruction is enabled, until the FIFO is full.
IMPORTANT: You must test and confirm that the instruction does not change data that you don’t want it to change.
The FFL instruction operates on contiguous memory.
The data is constrained by the specified member.
If the instruction tries to read past the end of an array, the instruction generates a major fault.
Typically, the Source and the FIFO are the same data type. If Source and FIFO data types mismatch, the instruction converts the Source value to the data type of the FIFO tag.
A smaller integer converts to a larger integer by sign-extension.
Available Languages
Ladder Diagram
Ladder Diagram_FIFO Load (FFl)_v1
Operands
Conversion only occurs if the type of the source operand does not match the type of the FIFO.
Ladder Diagram
Operand
Type
Format
Description
Source
SINT
INT
DINT
REAL
String type
structure
immediate
tag
Data to be stored in the FIFO
FIFO
SINT
INT
DINT
REAL
String type
structure
array tag
FIFO to modify
Specify the first element of the FIFO
Control
CONTROL
tag
Control structure for the operation
Typically use the same CONTROL as the associated FFU
Length
DINT
immediate
Maximum number of elements the FIFO can hold at one time
Position
DINT
immediate
Next location in the FIFO where the instruction loads data
initial value is typically 0
CONTROL Structure
Mnemonic
Data Type
Description
.EN
BOOL
The enable bit indicates the FFL instruction is enabled.
.DN
BOOL
The done bit is set to indicate that the FIFO is full. The .DN bit inhibits loading the FIFO until .POS < .LEN.
.EM
BOOL
The empty bit indicates the FIFO is empty. If .LEN is < or = to 0 or .POS < 0, the .EM bit and .DN bits are set.
.LEN
DINT
The length word specifies the maximum number of elements in the FIFO.
.POS
DINT
The position word identifies the location in the FIFO where the instruction loads the next value.
Affects Math Status Flags
No
Major/Minor Faults
A major fault will occur if:
Fault Type
Fault Code
The (starting element + .POS) is past the end of FIFO array
4
20
See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
See the FFL Flow Chart (Prescan).
Rung-condition-in is false
See FFL Flow Chart (False)
Rung-condition-in is true
See FFL Flow Chart (True)
Postscan
N/A
FFL Flow Chart (Prescan)
RSL5K_FFL Flow Chart Prescan
FFL Flow Chart (False)
RSL5K_FFL Flow Chart False
FFL Flow Chart (True)
FFL Flow Chart True
Examples
Example 1
Ladder Diagram
FTStudio-FFL-LD-EX1-V1
FFL Example 1
Example 2
Source array is STRING array or Structure array.
Ladder Diagram
FTStudio-FFL-LD-EX2-V1
Example 3
Data type of source mismatch data type of FIFO array.
Ladder Diagram
FTStudio-FFL-LD-EX3-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal