Loading

Arena Simulation Software in Packaging

Model and Predict Performance in Your Packaging Process
World Map centered in virtual environment
Arena Simulation logo
    • 개요
    • Call Center
    • Call Center
    • Food & Beverage
    • Food & Beverage
    • Government & Military
    • Government & Military
    • Healthcare & Hospital
    • Healthcare & Hospital
    • Logistics
    • Logistics
    • Manufacturing
    • Manufacturing
    • Mining
    • Mining
    • Oil & Gas
    • Oil & Gas
    • Packaging
    • Packaging
    • Port & Terminal
    • Port & Terminal
    • Retail
    • Retail
    • Supply Chain
    • Supply Chain
    • Case Studies
    • Case Studies
  • Arena Software in Academics
    • 개요
    • FAQs
    • FAQs
    • System Requirements
    • System Requirements
    • Training Services
    • Training Services
    • Consulting Services
    • Consulting Services
    • 개요
    • Find a Distributor
    • Find a Distributor
    • Software Download Options
    • Software Download Options
    • Case Studies
    • Case Studies
    • Blog
    • Blog
Download Free Trial

Design your packaging system correctly the first time including conveyor lengths, accumulation sizing and sensor positions. Arena Simulation Software enables you to model and predict system performance based on key metrics such as throughput, utilization, blockages/starvations and effective run rates.

Packaging lines can be tasked with processing hundreds or even thousands or products per minute. A multitude of variables impact the performance of these systems—including machine speeds, conveyor speeds, and capacity—and failure to meet required demands can compromise production. Improving performance and reducing downtime requires a robust solution that factors in multiple variations and system interactions—a task which is almost impossible to accomplish using spreadsheet analysis.


What is Packaging Optimization?

Packaging optimization is a computer-based model of the packaging process that enables you to simulate packing line operation in a virtual world before implementing modifications in the real world. These models incorporate system interactions, resource requirements and process variability into the simulation to provide a realistic view of packing operations. These models enable organizations to address important issues like the following:

  • Impact of changing machine speeds and downtimes
  • Impact of conveyor speeds and accumulation capacity
  • Operator requirements to meet machine changeover and machine downtime events
  • Effect of variation due to downtime and changeover on system operation
  • Impacts of the line control system

Effective optimization requires simulation, and that’s where Arena can help.

Arena is the leading global business process simulation solution, which gives packaging engineers the ability to create models that can be tested and adjusted quickly without any programming experience. Implementing an optimization strategy using models lowers cost, saves time, and decreases the risk often associated with the standard trial-and-error approach.

Arena is the world's leading discrete event simulation platform, serving the majority of Fortune 100 companies.

Features and Capabilities

Easy-to-Build a Packaging Process Flow

  • Build a packaging process flow in a fast, intuitive and easy-to-learn manner
  • Drag and drop elements and structures allow you build simulations and visualize results
  • Engaging 2D and 3D animation capabilities that do not require programming assistance

Dashboards for Packaging Optimization

  • Built-in dynamic dashboards provide the model analysis you need to facilitate packaging optimization
  • Build customized displays of the model information to enable you to better understand what is happening in your process

Common Capabilities

  • Increased throughput
  • Eliminate blockages/starvations
  • Optimize equipment utilization
  • Test new process configurations before implementing in the plant

Plant Simulation Software

Successful plant operation requires that multiple process operations are coordinated to work at maximum efficiency. If your production line is unbalanced, the result can be increased WIP, higher off-grade material and a reduction in plant throughput. Logistics inefficiencies can also increase costs when production must stop due to resource constraints or available storage capacity. Simulation can help you optimize your plant processes to reduce costs and improve throughput.


What is Plant Simulation?

Plant simulation software allows you to create digital models of your production processes to improve how each process interacts with, transitions to, and is affected by the next process. For example:
  • Manufacturing: model the interactions and variability between systems and resources. Determine inefficiencies and bottlenecks as well as the ways downstream operations can impact production.
  • Packaging: model the effects of adjustments to machine or conveyor speeds, as well as system downtime and maintenance.
  • Logistics: determine how scheduling or resource allocation affects efficiency with receiving, distribution, and warehousing.

Related Industries

Loading
Loading
Loading
Loading

Case Studies

정렬 및 필터
필터 및 정렬
정렬 기준
Showing {0}-{1} of {2} Results
정렬 기준:
페이지당 항목 수:
{0}-{1} of {2}
  1. Chevron LeftChevron Left Rockwell Automation 홈 Chevron RightChevron Right
  2. Chevron LeftChevron Left 제품 Chevron RightChevron Right
  3. Chevron LeftChevron Left 소프트... Chevron RightChevron Right
  4. Chevron LeftChevron Left Arena Simulation Software Chevron RightChevron Right
  5. Chevron LeftChevron Left Discrete Event Modeling Chevron RightChevron Right
  6. Chevron LeftChevron Left Arena Simulation Software in Packaging Chevron RightChevron Right