Shock Events
PowerFlex®
755T products can withstand a finite number of shock events. The maximum allowable number of shock events increases as the peak amplitude decreases. Below 0.7 g peak, the maximum total shock events should not exceed 2000 cycles.Shock Events Graph
Provide Feedback