Remove and Install the Wire Bay Thermal Switch for Frames 8...15

Replace the thermal switch with kit catalog number SK-RM-THRMSW-WB. Follow these steps to remove and install the thermal switch.
  1. Review the product advisories in Before You Begin.
  2. Remove power from the system.
  3. Open the wire bay enclosure door.
  4. Loosen the 12 screws that secure the guards to the enclosure and remove the guards.
    example of how to remove the entry/exit wire bay guard
  5. Remove the two M6 x 25 mm Torx screws that secure the thermal switch assembly to the mounting bracket on the bus bar and remove the assembly. Retain the screws, guard, and clamp for reuse.
  6. Disconnect the wires from the two terminals on the thermal switch.
    example of how to remove the thermal switch from a wire bay
  7. Install the thermal switch in the reverse order of removal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal