Remove and Install the AC Precharge Time Delay Relay for Frames 8...15
Replace the AC precharge time delay relay with kit catalog number 20-750-MACPC-TDR. Follow these steps to remove and install the AC precharge time delay relay.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Open the input bay enclosure door.
- Remove the guard from the enclosure.
- Disconnect the wires from the top terminals on the time delay relay.
- Pull up on the bottom of the relay chassis and lift it up and off the DIN rail.
- Install the AC precharge time delay relay in the reverse order of removal.
Provide Feedback