Remove and Install the Control Pod Cover for Frame 7
You must remove the control pod cover to access other components inside the pod. Follow these steps to remove and install the control pod cover.
- Review the product advisories in Before You Begin.
- Remove power from the system.
- Open the enclosure door.
- Loosen the two captive screws at the top of the control pod and pull the cover out from the chassis.
- Lift the bottom of the cover off the tabs (A) and remove the cover.
- TIP: The control pod Is shown separated from the power bay to clarify the instructions only.
- Install the control pod cover in the reverse order of removal.
Provide Feedback